A powerful tool for molecular analysis and real-time process insight
ArticleVíce odvětví11.07.2025
Ve zkratce
Definition: Raman spectroscopy is a molecular spectroscopy technique that detects changes in molecular vibrations, offering a unique “molecular fingerprint” for chemical identification.
Benefits: Enables non-destructive, real-time, in situ analysis with minimal sample prep. Ideal for aqueous systems, quantitative monitoring, and process control.
Applications: Used across pharmaceuticals, bioprocessing, polymers, specialty chemical production, refining, food and beverage production, and more; key enabling technology for new energies and carbon capture, utilization, and storage.
Technology: Raman systems integrate lasers, probes, optics, and detectors to deliver highly specific chemical data for both qualitative and quantitative analysis.
ObsahObsah
What is Raman spectroscopy?
Spectroscopy is an analytical technique that uses UV, visible, or infrared light to measure chemistry. It provides fast, label-free, non-invasive, and non-destructive chemical analysis of a material. Focused beam reflectance measurement (FBRM), ultraviolet/visible (UV/Vis), near-infrared (NIR), infrared (IR), and Raman are examples of spectroscopy widely used in industrial R&D or process environments.
Within this toolbox, vibrational spectroscopy techniques—including NIR, IR, and Raman—are powerful tools for understanding composition and molecular structure. NIR uses near-infrared radiation, IR uses infrared radiation, and Raman uses visible or near-infrared radiation to measure chemical composition and molecular structure.
Vibrational spectroscopy is especially valuable because it provides specific chemical information without requiring extensive sample preparation. Raman spectroscopy, a type ofvibrational spectroscopy that provides a highly specific molecular fingerprint, is similar to IR. However, there are differences between Raman and IR that influence where they are used in industrial applications.
Differences between IR and Raman spectroscopy
One key difference between infrared and Raman spectroscopy is how water affects the spectrum. Water strongly absorbs infrared light, often obscuring IR signals from a sample. In contrast, water has a weak Raman signal, making Raman spectroscopy better suited for measurements in aqueous solutions. Another difference lies in the wavelengths used: Raman spectroscopy employs visible or near-infrared wavelengths, allowing the use of standard optical fibers and detectors. However, IR spectroscopy requires specialty fibers and detectors due to its use of infrared wavelengths. This makes Raman spectroscopy ideal for remote monitoring and installations where the detector and probe are separated by longer distances.
How Raman spectroscopy works
When light interacts with a molecule, it can be refracted, absorbed, or scattered. In scattering, most photons do not interact with a molecule and simply “bounce” off it. This is known as Rayleigh or elastic scattering. A small fraction of light undergoes inelastic scattering, where photons interact with molecular vibrations or rotations, resulting in energy shifts. These shifts form a Raman spectrum, which serves as a molecular fingerprint. Most Raman spectroscopy instruments measure these molecular vibrations.
The collected light is interpreted as a spectrum by the camera, creating a “molecular fingerprint” of the sampled material.
Raman scattering
Raman scattering Discovered in 1928 by C.V. Raman and K.S. Krishnan, Raman scattering describes how a small portion of light scattered by a molecule changes frequency due to energy transfer with molecular vibrations. The first Raman studies were performed using sunlight as the light source and photographic equipment. The “excessive feebleness of the effect” was acknowledged in the original paper by Raman and Krishnan. It was not uncommon for researchers to spend hours or even days collecting a single spectrum. The advent of lasers, sensitive detectors, and fast holography-based optics has improved the speed, resolution, and sensitivity of Raman spectroscopy. Today, a single Raman spectrum can be measured in minutes or even seconds.
The scattering process When a photon interacts with a molecule, it may excite an electron to a virtual energy state. If the electron returns to a different vibrational level, the scattered photon has a different energy, based on the initial energy of the molecular vibration.
Stokes scattering: Photon loses energy (most common)
Anti-Stokes scattering: Photon gains energy (less intense)
These energy differences are plotted as Raman shifts in wavenumbers (cm⁻¹) in a spectrum. Because molecules have many vibrations, each with different energies, these shifts provide information about various functional groups within the molecule.
Vibrational energies and selection rules
Vibrational energies Vibrational energy depends on several molecular properties:
Atomic mass
Bond order
Molecular geometry
Hydrogen bonding
Raman spectroscopy can measure various compositional and structural aspects of a molecule, including both backbone and side chains, making it valuable in fields such as materials science, polymers, edible oils, and biochemistry.
Selection rules A vibration is Raman-active if it causes a change in polarizability. Typically, symmetric stretches or vibrations are Raman active. This mechanism complements IR spectroscopy, where a vibration must change the dipole moment and typically involves asymmetric vibrations.
Strong Raman scatterers: Molecules with delocalized electron clouds (e.g., C=C bonds)
Weak scatterers: Highly polar bonds (e.g., O–H)
Advanced Raman techniques
Variations of Raman spectroscopy continue to be developed to enhance the Raman signal or reduce fluorescence interference. Two important enhancement approaches are Resonance Raman and Surface-Enhanced Raman Scattering.
Resonance Raman (RR) When the excitation laser matches an electronic transition, certain vibrational modes are resonantly enhanced—by factors of 10² to 10⁴. This technique is useful for studying chromophores and aromatic compounds.
Surface-Enhanced Raman Scattering (SERS) SERS enhances Raman signals by 10³–10⁶× when molecules are adsorbed on nanostructured metal surfaces (e.g., silver, gold). It enables detection of micromolar concentrations, though its use is limited by surface chemistry and adsorption kinetics.
Qualitative vs. quantitative Raman
Historically, Raman was used for qualitative analysis—identifying chemical species by their spectral fingerprints. However, advances in holographic technology, high-throughput analyzers, and multivariate data analysis have enabled quantitative Raman spectroscopy.
Qualitative: Identifies compounds
Quantitative: Measures concentrations in real time
Since its introduction to industrial settings in the mid-1990s, Raman spectroscopy based on modern dispersive instrumentation has been used to solve challenges in identification, quantification, and process monitoring. Early applications were closely linked to those already analyzed by Fourier-transform infrared spectroscopy (FTIR) or FT-Raman, as Raman provides similar compositional and molecular structure information.
In many of those early reports, Raman was tested only after the implementation limitations of FTIR or FT-Raman—such as sample probe fouling, high laser power, or incompatibility with aqueous systems —became apparent. Following initial successes, industrial confidence in the Raman technique and the robustness of its hardware grew, leading to broader adoption for Raman-based product or process understanding.
Today, Raman spectroscopy is proven to provide the specificity of FTIR with the measurement ease of NIR spectroscopy. A modern perspective views Raman as a first-choiceProcess Analytical Technology (PAT), rather than as a PAT of last resort.
Because Raman spectroscopy uses visible or near-infrared light, it can be coupled to many different types of instruments. Raman spectra can be measured using dispersive instrumentation coupled with a microscope, handheld or portable unit, or fiber-optic measurement probes.
Raman applications across phases of matter and industries
Raman spectroscopy is a versatile analytical tool used across solids, liquids, gases, and complex media—supporting a wide range of industries and research fields.
Phases of matter Raman spectroscopy can be applied to a broad range of materials, including:
Industry applications Raman spectroscopy plays a critical role in numerous industry sectors, including:
Pharmaceuticals: API reaction monitoring, solid dose processing, polymorph identification, formulation optimization, PAT
Bioprocessing: Upstream cell culture monitoring and control, higher order structure, media prep, target protein concentration, product formulation, PAT
Industrial Forensics: Defective material identification, polymorph identification, aggregates, adulteration
Semiconductors: Stress/strain analysis, material characterization
Specialty Chemical: Ammonia synthesis, methanol production, fine chemical reaction monitoring, crystallization, olefin production
Environmental & Geological Sciences: Carbon capture, utilization, and storage
Food & Beverages: Edible oil quality, chocolate, cultivated meat, adulteration, fermentation monitoring and control
Oil & Gas: Refining, amine sweetening, natural gas production
Expanding frontiers Today, the answer to the question of whether a measurement problem may be well suited to Raman spectroscopy is generally “yes.” Hardware reliability, a myriad of sample measurement modalities, model transferability, and low operational costs make Raman spectroscopy an attractive analysis tool. As Raman spectroscopy continues to evolve, new advancements in instrumentation and applications are expanding its impact across research, clinical, and laboratory settings. Emerging uses include biomedical fields such as tissue analysis and disease diagnosis, as well as art conservation through pigment and material identification.
Frequently asked questions about Raman spectroscopy
Chcete se zúčastnit jedné z našich akcí? Vyberte podle kategorie nebo odvětví.
Vážíme si vašeho soukromí
Soubory cookie používáme k vylepšení vašeho zážitku z prohlížení a shromažďujeme statistiky za účelem optimalizace funkčnosti webu, abychom vám mohli poskytnout reklamy nebo obsah na míru.
Výběrem možnosti „Přijmout vše“ souhlasíte s naším používáním souborů cookie.
Další podrobnosti naleznete v našich Zásadách používání souborů cookie .